Bourns Introduces TVS Diode Products Featuring High Peak Power and Current Ratings to Protect Sensitive Electronics

RIVERSIDE, Calif., October 22, 2019 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today introduced its Model 15KPA-SD-Q transient voltage suppressor (TVS) diode series. Bourns designed its latest TVS diodes for use in DC bus clamping applications, and to protect sensitive electronics applications against overvoltage transients. In addition, these new protection devices are AEC-Q101- compliant making them ideal protection solutions for applications that require high reliability such as in power supplies and equipment used in harsh environments.

The Model 15KPA-SD-Q Series offers superior performance from its high peak pulse power (10/1000μs) rating of 15kW and high peak pulse current (8/20 μs) rating of 1kA. These new protection components also feature lower clamping voltage under surge, performance stability and increased reliability compared to competing metal oxide varistor (MOV) technology.

The Bourns® Model 15KPA-SD-Q Series comes in a surface-mount DO-218AB package well-suited for automated pick and place assembly and reflow processes. Manufacturing production costs can be reduced and PCB assembly is simplified using surface-mount components compared to similar products with traditional through-hole packages.

Available now, Bourns® Model 15KPA-SD-Q Series is RoHS* compliant and halogen free**. For additional product information, please see: www.bourns.com/products/diodes/diodes-aec-q101-compliant

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

ボーンズ社について

ボーンズ社(Bourns, Inc.) は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf

メディアエージェンシー窓口:
Annette Keller
Keller Communication
(949) 947-7232
annettekeller1984@gmail.com
弊社窓口:
Josephine Chen
Bourns Asia Pacific, Inc.
886-2-2562-4117 #138
Josephine.chen@bourns.com
Keyword
Data Sheet
Inventory
RoHS