Search
Languages

Bourns Announces New Sulfur-Resistant Fixed Resistor Series

RIVERSIDE, Calif., June 24, 2019 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced a new sulfur-resistant AEC-Q200 compliant thick film resistor family. The Bourns® Model CRxxxxA-AS chip resistor series is offered in eight different footprints from small 0201 (0603 metric) to 2512 (6432 metric) with rated power from 0.05 to 1 watt. The new surface-mount chip resistors also feature a wide resistance range from 1 ohm to 20 megohms making them ideal for a variety of general-purpose applications.

Bourns designed these resistors to operate in certain harsh environments with higher levels of sulfur contamination. They are manufactured using a thick film element printed onto a ceramic substrate, and tested in accordance with ASTM B809-95 methods, which tests for the porosity of metallic coatings exposed to humid sulfur vapor.

Available now, the Model CRxxxxA-AS chip resistor series complements the other circuit conditioning components from Bourns that include power inductors and rectifier diodes. Bourns' expanded line of sulfur-resistant fixed resistors are RoHS* compliant and halogen free**. For additional product information, please see the datasheet on the Bourns website: www.bourns.com/docs/product-datasheets/crxxxxa-as.pdf.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

***Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

ボーンズ社について

ボーンズ社(Bourns, Inc.) は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf