Search
Languages

At China International Battery Fair 2018, Bourns to Showcase Full Line of Protection Solutions for Consumer Electronics Batteries

RIVERSIDE, Calif., May 17, 2017 - Bourns, Inc., a leading manufacturer and supplier of electronic components, offers essential protection components for consumer batteries and automotive battery management systems. At the China International Battery Fair 2018, Bourns will display its latest series of high current mini-breaker thermal cutoff (TCO) products engineered to provide superior overtemperature and overcurrent protection for notebook and tablet PC battery cells. The new Bourns® Model AC series builds on the success of the Model AA series launched in January 2017 offering multiple improved features to meet the next-generation protection needs of denser, higher capacity Lithium-Ion (Li-ion) battery cells. In addition, the Model AC series offers a fifth trip temperature option of 90 °C, and is capable of carrying up to 20 A at 60 °C, making it the highest current-carrying TCO device Bourns offers.

Attendees will also see Bourns' surface mount SA series TCO devices. The Bourns® Model SA series is designed to help battery pack suppliers greatly reduce lead times and assembly costs. These are the latest products added to Bourns' already broad line-up of TCO products proven in more than 2 billion existing battery cells

Where: China International Battery Fair, Shenzhen Convention & Exhibition Center
When: May 22 – 24, 2018
Location: Bourns Booth #2T070

To schedule a meeting with a Bourns battery protection expert, please contact Josephine Chen: +886-2-2562-4117 ext: 138, josephine.chen@bourns.com.

ボーンズ社について

ボーンズ社(Bourns, Inc.) は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf