Search
Languages

Bourns Expands Multifuse PPTC Line with Smaller Size Models Offering Extended Operating Current

RIVERSIDE, Calif., April 12, 2017 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced the expansion of its successful MF-RG Series Multifuse® Polymer Positive Temperature Coefficient (PPTC) Resettable Fuse product line. The eight new MF-RG Series models extend the maximum operating current of the series from 3 A to 11 A, and are a smaller size compared to Bourns' existing through-hole Multifuse® products (MF-R, MF-RX), thus delivering a space saving and thermal advantage resulting in a higher performing circuit protection solution.

These radial through-hole PPTC MF-RG products are rated to a maximum operating voltage (Vrms) of 16 V offering high current-carrying capability. The new MF-RG models feature a tighter hold to trip ratio that operates much closer to the fault current of the application, thereby delivering a faster response solution for overcurrent events. The smaller size with a similar Ihold rating and fast tripping capabilities make Bourns' latest Multifuse® devices excellent circuit protection solutions for a broad variety of automotive, industrial and communications market applications.

The Model MF-RG Multifuse® PPTC products are manufactured in Bourns' TS16949 approved facility, and are RoHS compliant*, UL recognized for safety requirements, and meet AEC-Q200 compliance standards for passive components.

Pricing and Availability
All eight new models in the MF-RG Series are available now. For more information, please go to: www.bourns.com/products/circuit-protection/resettable-fuses-multifuse-pptc

ボーンズ社について

ボーンズ社(Bourns, Inc.) は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf