Search
Languages

Bourns Announces New Low Profile TVS Diode

Riverside, Calif., November 19, 2013 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced the availability of its new low profile transient voltage suppressor (TVS) diode, designated Bourns® Model CDDFN2-T3.3B. Bourns designed its new low capacitance (13 pF) diode in a smaller surface mount package as an optimal ESD, EFT and surge protection solution. The new TVS diode provides reliable circuit protection for external ports in a broad range of electronic devices such as computers and peripherals, communication systems, cellular phones, handheld portable electronics and audio and video equipment.

The Bourns® Model CDDFN2-T3.3B TVS diode is tested to IEC protection standards — IEC 61000-4-2 (ESD), IEC 61000-4-4 (EFT) and IEC 61000-4-5 (Surge). This latest low profile diode measures only 1.0 mm x 0.60 mm x 0.55 mm and is available in a DFN-2 package. It is designed to be mounted directly onto an FR4 printed circuit board, and its package size meets the surface mount component 0402 footprint. "Not only does our new low profile TVS diode offer superior standards-based ESD, EFT and surge protection, its smaller surface mount package helps designers meet ever-smaller board space constraints and higher integration requirements," said Ben Huang, Product Line Manager, Semiconductors at Bourns, Inc. "This device is intended to replace Bourns® Model CDDFN2-T3.3LC surface mount TVS Diode, which was recently obsoleted."

Pricing and Availability
As a pricing reference, the Bourns® Model CDDFN2-T3.3B is priced from $0.13 in 12,000 piece quantities, is available now and is RoHS compliant*. For additional product information and specifications, please go to: www.bourns.com/en/docs/product-datasheets/CDDFN2-T3.3B.pdf

ボーンズ社について

ボーンズ社(Bourns, Inc.) は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf