Search
Languages

Bourns Announces New SMD Power Inductor Series for Use in Automotive Applications

Riverside, Calif., September 17, 2013 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today introduced its SMD Power Inductor Series that includes 13 new models. The new series features non-shielded and shielded construction and is AEC-Q200 qualified. Bourns' new SMD power inductor models are specifically designed for use in a broad range of automotive applications that include driver assistant devices, information/entertainment systems and lighting.

"Bourns' new series of SMD power inductors feature non shielded as well as shielded construction as requested for today's advanced automotive systems with AEC-Q200 testing," said Guido Zehnder, Magnetics Product Line Manager at Bourns, Inc. "These high-performance power inductors meet the needs of complex automotive applications and provide customers with solutions they can count on for reliability and longevity."

Pricing and Availability
Bourns® Models SDE1006A, SDR1307A, SRF1260A, SRR0735A, SRR1260A, SRR1280A, SRU1028A, SRU1038A, SRU1048A, SRU3028A, SRU5028A, SRU6025A and SRU8028A are available now. For additional product information, go to bourns.com/en/docs/product-datasheets/Bourns_IC1326_Automotive_Inductor_FPB.pdf. As a pricing reference, the new SMD power inductors are priced from $0.23 to $0.39 each per 2,000-piece order. The new models are also RoHS compliant* and halogen free**.

 *RoHS Directive 2002/95/EC Jan. 27, 2003 including annex and RoHS Recast 2001/65/EU June 8, 2011.

**Bourns follows the prevailing definition of “halogen free” in the industry. Bourns considers a product to be “halogen free” if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (BR) and Chlorine (Cl) content is 1500 ppm or less.

ボーンズ社について

ボーンズ社(Bourns, Inc.) は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf