Search
Languages

Bourns Announces Availability of Two New Evaluation Boards for RS-485-based Applications

Riverside, Calif., August 3, 2011 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced the availability of two new evaluation boards for RS-485-based applications. Using Bourns® TBU® High-Speed Protectors (HSPs), GDTs, TVS diodes and MOV products, the new boards were developed as a design resource that streamlines evaluating circuit protection on RS-485 serial device ports. To meet the required industry standards on RS-485 port interfaces, the new boards provide two different evaluation approaches. The Bourns RS-485EVALBOARD1 includes two Bourns® TBU® High-Speed Protectors (HSPs), two Bourns® fast-acting GDTs and two Bourns® TVS diodes. The Bourns RS-485EVALBOARD2 uses Bourns® TBU® High-Speed Protectors (HSPs), MOVs and TVS products.

"Bourns designed the evaluation boards to help developers more quickly and easily determine the circuit protection required for their applications that use RS-485 serial device ports," said Ian Doyle, product line manager of semiconductor products at Bourns, Inc. "The evaluation boards demonstrate that with Bourns® TBU® HSP solutions, we are able to offer enhanced performance features over competing technologies in terms of increased surge and transient protection levels on RS-485 ports that also enable an entire circuit protection solution to fit into a smaller PCB area."

Bourns' RS-485 evaluation boards are offered through the company's distribution sales partners, with inventory available immediately at Digi-Key, Farnell and Mouser. As a pricing example, the Bourns RS-485EVALBOARD2 is priced at $20.00 in 10 piece quantities.

For more information, Bourns has produced a demonstration video that explains the use and benefits of its RS-485 evaluation boards in assessing port protection performance: https://www.youtube.com/watch?v=dvCscFwlM_w

ボーンズ社について

ボーンズ社(Bourns, Inc.) は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf