Search
Languages

Bourns Announces Combined Torque and Angle Sensor for Electric Power Assisted Steering Applications (EPAS)

Riverside, Calif., May 10, 2011 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced a new combined torque and angle sensor designed for Electric Power Assisted Steering Applications (EPAS) and other automotive systems. The new combined sensor provides torque and steering angle measurement in a single package, replacing two discrete sensors for significant space and cost savings. Based on Bourns’ Hall Effect (HE) non-clockspring torque sensor technology, the combined sensor uses driver input to measure the steering torque while simultaneously converting the rotation speed and direction of the steering wheel. The torque portion of the sensor is designed specifically for EPAS, and the steering angle signal can be used in a variety of automotive systems including Electronic Stability Control (ESC), Advanced Front Lighting Systems (AFLS), Navigation, and Assisted Parking Systems.

"Bourns has more than 14 years experience in delivering proven steering angle and torque sensors, and is committed to continued innovation,” said Johneric Leach, product line manager for steering and vehicle stability sensors at Bourns. “Using this experience to combine technologies into a single functional package demonstrates our innovation, and Bourns has made a significant investment in extensive trials and testing to ensure this product meets customer expectations and next-generation automotive requirements.”  

Bourns offers several variations of its new combined torque and angle sensor to meet customer requirements. Variations include dual and single channel options on the torque portion depending on redundancy requirements, and the steering angle sensor can support incremental or absolute measurement. The new Bourns® torque and angle sensor is suitable for column or rack mounted EPAS. For rack-mounted applications, the combined sensor has been designed to sustain temperatures from -40°C to +125°C.  The new device provides CAN steering sensor output in addition to an analog torque signal. The torque sensor output can also be configured to support CAN, analog, PAS4, PSI5 and PWM outputs.

Bourns will make its combined torque and steering angle sensor available to a select group of customers. Product validation is currently being conducted with two of the world’s largest EPAS suppliers.

ボーンズ社について

ボーンズ社(Bourns, Inc.) は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf