Search
Languages

Bourns Announces New Line of Shunt Protectors Designed Specifically for Sensitive LED Lighting Applications

Riverside, Calif., February 15, 2011 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced a new line of open LED shunt protection devices designed specifically for LED lighting applications. Designated the Bourns® LSP-Series, the new shunt protector family enables LED lighting applications configured in strings to be more robust and reliable. Most LED designs include solid-state lighting luminaries configured in series strings of 20 or more LEDs. In this configuration, an open LED can cause the entire LED string to go dark, resulting in reduced performance and possible maintenance calls and costly warranty returns. Adding a Bourns® LSP-Series shunt protector to an LED design allows the unaffected lights in the string to remain illuminated by shunting current around the inoperable LED. The new LSP-Series of open LED shunt protectors are an optimal solution for a variety of LED lighting applications including light bulbs, lighting fixtures and backlighting systems.

"LED lighting applications are exploding in volume," said Ian Doyle, product line manager of semiconductor products at Bourns, Inc. "Bourns' new LSP-Series of open LED shunt protectors address the failure rates of early LED designs. Incorporating a Bourns® LSP device into the design of LEDs improves reliability and helps eliminate costly downtime."

The Bourns® LSP-Series of open LED shunt protectors include four models: LSP0600BJR-S, LSP0900BJR-S, LSP1300BJR-S and LSP1800BJR-S. Customers can maximize the level of protection by selecting Bourns® model LSP0600BJR-S and using one device per LED. Alternatively, customers can reduce their protection costs by selecting Bourns® models LSP0900BJR-S, LSP1300BJR-S or LSP1800BJR-S that are able to isolate groups of two, three or four LEDs respectively. Bourns' new device family comes in an SMB surface mount package and is RoHS* compliant. Product samples are available now through Bourns' distribution partners. As a pricing example, Bourns® LSP0600BJR-S is priced at $.30 each in 10K piece quantities.

*RoHS Directive 2002/95/EC January 27, 2003 including Annex.

ボーンズ社について

ボーンズ社(Bourns, Inc.) は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf