Search
Languages

Bourns Adds New Ultra-Low Capacitance Thyristor Surge Protectors to its TISP® Product Line

Riverside, Calif., March 23, 2010 Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced that the company has expanded its TISP® thyristor surge protector product line to include new ultra-low capacitance models that allow higher data rates to deliver improved VDSL2 performance while providing protection. The new Bourns® Models TISP4P015L1N, TISP4P020L1N, TISP4P025L1N and TISP4P035L1N address a range of popular chipset voltages. These new thyristor surge protectors are designed with a new lower capacitance process as an optimal circuit protection solution for ADSL, ADSL2, ADSL2+, VDSL and VDSL2 applications from overvoltages caused by lightning and AC line disturbances. Low capacitance reduces distortion and minimizes the effect of using circuit protection in sensitive equipment. The new devices can also be used for T1/E1 driver protection, in customer premise and central office locations and in any transformer-coupled interface, which leaves the building.

Bourns new TISP® devices are symmetrical, two-terminal thyristor-crowbar devices that can be deployed to protect from line to ground or between the differential driver conductor pair. When placed between the xDSL line driver IC and the transformer, the devices will clamp and switch into an ultra-low impedance state, safely diverting the energy and protecting sensitive equipment from dangerous overvoltage or line disturbance threats that can result in system failure.

"These new models offer significant competitive advantages for our customers,” said Beverley McKnight, product line manager for Bourns’ TISP® products. “These new protectors feature differential capacitance, typically less than 3 picofarad (pF), which makes them our lowest capacitance device. They enable reliable overvoltage protection that meets the faster data rates required by a broad range of VDSL2 applications. Bourns designed these new TISP® products to help our customers deliver high reliability and low cost solutions for their faster data rate products.”

Pricing and Availability
Bourns® Models TISP4P015L1N, TISP4P020L1N, TISP4P025L1N and TISP4P035L1N are available now. For complete specifications, go to Bourns’ website at  TISP. As a pricing reference, the new models are priced from $0.30 at 10,000 pieces.

ボーンズ社について

ボーンズ社(Bourns, Inc.) は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf