Search
Languages

Bourns Introduces New WEBENCH-Based Tools for Power Supply, LED Driver Design and Inductor Selection

Riverside, Calif., November 17, 2009 Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced that the company has introduced the availability of WEBENCH® Designer customized specifically for Bourns and its inductor customers. In cooperation with National Semiconductor Corp., the Bourns® version of WEBENCH Designer is available now on the Bourns website, www.bourns.com. It is a powerful design and prototyping tool designed to help create power supplies, DC-DC converters and LED driver solutions that meet design requirements for simulation, optimization and quick prototypes. WEBENCH tools enable designers to easily fine-tune switching power supply and LED driver designs and solve problems before a prototype is built, alleviating the time and extra costs associated with traditional design methods. The new toolset can also be used for device selection allowing customers to locate the optimal switching regulator and Inductor products for their power supply and LED applications.

&;quot;One of the great challenges of power supply design is finding the time to perform labor-intensive tasks to define the circuits and calculate component values,&;quot; said Andy Chow, Field Application Engineer for Bourns, Inc. &;quot;Bourns now offers an easy-to-use, advanced toolset to automatically create the best possible power supply to meet both designer and customer requirements in just a few keystrokes and every solution is optimized around the ideal Bourns Inductor.&;quot;

To use the new Bourns version of WEBENCH Designer, simply log onto the Bourns website and click on the &;quot;LED and Power Design Tool&;quot; caption on the home page. Visitors are then asked to enter their input voltage, the desired output voltage and current for their power supply. WEBENCH Designer displays several circuit solutions for power IC and Bourns Inductor options, including recommendations for the surrounding components.

The optimization tool allows designers to fine-tune their design by making tradeoffs between efficiency and footprint. After the schematic is finalized, the bill of materials (BOM) presents the ideal Bourns Inductor and all of the other power components in the system. Adding to the inductor selection flexibility, &;quot;Select Alternate Part&;quot; allow designers to choose another Bourns Inductor for a different footprint or performance. A final printout featuring a full report including schematic, BOM, operating values, and performance charts is also available. Over 1900 Bourns Inductors are included in the tool, providing solutions to a large variety of applications. The parametric values cover a wide range including: Inductance from .1 µH to 15000 µH, DCR&;#39;s from 2 mOhms to 168 Ohms and Current rating from 20mA up to 46A

Bourns® and the Bourns logo are trademarks or registered trademarks of Bourns, Inc. and may be used only with the permission of Bourns and proper acknowledgement.

WEBENCH is a registered trademark of National Semiconductor Corporation and used with permission.

ボーンズ社について

ボーンズ社(Bourns, Inc.) は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf