Search
Languages

Bourns Announces New Series of Surface Mount GDT Surge Protectors Designed for Broadband Protection

Riverside, Calif.,, August 13, 2009 Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced a new series of three-electrode surface mount Gas Discharge Tube (GDT) surge protection devices ideal for broadband applications due to their ultra-low capacitance and low insertion and return loss performance. Designated the Bourns® 2054 Series, the robust devices are available in voltages from 230 to 470V and also feature RoHS* compliant versions. The Bourns® 2054 Series feature a compact size (5 x 7.2 mm) and offer superior protection characteristics suitable for a broad range of applications including telecommunications, commercial and industrial applications.

Bourns® GDTs help prevent damage from transient disturbances by creating a short-to-ground circuit during conduction. When an electrical surge exceeds the defined breakdown voltage level of the GDT, the device becomes ionized and rapid conduction takes place. When the surge passes and the system voltage returns to normal levels, the GDT returns to its high-impedance &;quot;off&;quot; state.

&;quot;GDTs are realizing growing market demand for use in broadband communication applications and Bourns is matching that need with its newest GDT 2054 Series for robust circuit protection in a cost-effective, compact package&;quot; said Craig Shipley, GDT products general manager for Bourns, Inc. &;quot;Bourns&;#39; new GDT devices provide excellent board-level protection of broadband applications and are also UL Recognized.&;quot;

Pricing and Availability
As a pricing reference, Bourns&;#39; 2054 Series is priced from $1.08 in 1-249 piece quantities and is available now. For a complete list of model numbers and characteristics, go to the 2054 datasheet.

*RoHs Directive 2002/95/EC Jan 27 2003 including Annex.

Bourns® and the Bourns logo are trademarks or registered trademarks of Bourns, Inc. and may be used publicly only with the permission of Bourns and require proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners.

ボーンズ社について

ボーンズ社(Bourns, Inc.) は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf