Search
Languages

Bourns Announces New Steering Diode Array Device Optimized for ESD, EFT and Surge Protection

Riverside, Calif., July 8, 2009 Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced the introduction of a new steering diode array that provides up to six lines of protection using the “rail to rail” clamping technique with low leakage current and low capacitance per line. Designated Bourns® model CDNBS08-SR112, the lead-free steering diode device was designed specifically for ESD, EFT and surge protection applications and is RoHS compliant.* Available in an NSOIC-8 package, the new device is designed to be mounted directly onto an FR4 printed circuit board. Bourns engineers optimized the design to protect a wide range of applications including Ethernet ports, portable electronics, wireless LANs and Universal Serial Bus (USB) interface-based systems.

Bourns’ steering diode array meets IEC 61000-4-2 (ESD), IEC 61000-4-4 (EFT) and IEC 61000-4-5 (surge) requirements for external ports and features very low capacitance of 5 pF to minimize electrical distortion. The devices also meet many worldwide, industry and government regulations regarding lead-free components and are designed for a variety of manufacturing environments, allowing the use of industry-standard “pick and place” equipment. The chip diode NSOIC-8 package offers simplified production with its flat configuration that minimizes rollaway.

"Bourns’ new steering diode array provides a good choice for ESD, EFT and surge protection for up to six communication data lines and also fits circuit board space constraints,” said Ian Doyle, ESD Product Line Manager for Bourns, Inc. “Bourns is pleased to offer the newest addition to the company’s steering diode array product line that meets industry demands for smaller electronic components with extremely low power consumption."


Electrical Characteristics (@ TA = 25 ºC Unless Otherwise Noted)
Parameter
Value
Typical Forward Voltage @ 50 mA (V)
1.3
Repetitive Peak Reverse Voltage (V)
20
Maximum Peak Pulse Current @ 8/20 µS (A)

12
Maximum Leakage Current @ 18 V (nA)

20
Typical Junction Capacitance @ 0 V 1 MHz (pF)
5
ESD Protection per IEC 61000-4-2
Minimum Contact Discharge (kV)
Minimum Air Discharge (kV)


±8
±15
EFT Protection per IEC 61000-4-4 @ 5/50 ns (A)

40
Surge Protection per IEC 61000-4-5 @ 8/20 µs
L1 (Line – Ground) (A)
L2 (Line – Line) (A)


12
12


Pricing and Availability
Bourns’ new steering diode array device is available now. As a pricing reference, Bourns’ CDNBS08-SR112 is priced from $0.90-$0.95 in 10,000 piece quantities.

*RoHs Directive 2002/95/EC Jan 27 2003 including Annex.

Bourns® and the Bourns logo are trademarks or registered trademarks of Bourns, Inc. and may be used publicly only with the permission of Bourns and require proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners. 


ボーンズ社について

ボーンズ社(Bourns, Inc.) は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf