Search
Languages

Bourns Announces Industry’s First ECL Triggered By Excessive Voltage or Current

Riverside, Calif., June 29, 2010 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced its latest series of Transient Blocking Unit (TBU™) circuit protection devices designed to protect telecommunications applications from surges in the industry’s first electronic current limiter triggered by excessive voltage or current. Designated the Bourns® TBU™ PL-Series SLIC, the new circuit protection device family provides extremely fast overcurrent protection combined with SLIC battery voltage tracking triggered protection. Combined with additional overvoltage protectors, this new solution protects against very high surge levels and meets telecom 500A Telcordia GR-1089 intrabuilding and 6kV/150A ITU-T standards.

Protecting sensitive telecom applications from the potentially damaging effects of surges that can cause current and voltage to rise above normal operating levels, the Bourns® TBU™ PL-Series responds in 100 nanoseconds. The resettable circuit protection devices also feature significantly lower let-thru energy and overshoot protection, which reduces stress on the SLIC and the printed circuit board (PCB) for increased reliability and product life. Bourns’ new TBU™ series also cuts the circuit protection component count to three devices compared to the seven needed in a conventional gated thyristor solution because there is no need for peripheral R-C or L-C components nor additional GDTs for increased surge requirements that take up valuable PCB space and increase manufacturing costs.

“Similarly, for customers who are currently using the Bourns® P-G TBU™ series, the new Bourns® TBU™ PL-Series drastically reduces the component count and the TBU™ package size is 25 percent smaller to better meet our customer’s needs for board area and height reductions,” said Paul Wiener, telecom market director at Bourns. “This new TBU™ series provides the best of both worlds – the highest protection levels with the fewest number of components.”

The Bourns® TBU™ PL-Series is available in three voltages (850, 600 and 500) and two operating current levels (100 mA and 200 mA) that match worldwide standards and SLIC chipset requirements. Product samples, evaluation boards and sample kits are available now through Bourns’ distribution partners. As a pricing example, Bourns® TBU-PL050-100-WH is priced at ($.056 each) in (3K) quantities.

關於美商柏恩(Bourns)

Bourns — 是電子零組件業界的龍頭製造供應商,公司總部位於美國加州的河邊市,其產品包含:位置與速度傳感器、電路保護解決方案、磁性組件、微電子模組、面板控制器及電阻產品,服務產業涵蓋汽車、工業、消費、通信、非關鍵性的生命支持醫療(低/中風險)、音頻以及其他各種市場。如需了解更多的公司與產品訊息,歡迎上公司網站查詢:www.bourns.com

Bourns®與Bourns標識為柏恩的註冊商標,惟有Bourns許可並取得適當的確認後才可使用。其他列出的名稱與品牌為其各自所有人的商標或註冊商標。

† Bourns®產品並非設計用於“救生”、“性命攸關”或“維持生命”應用,也不適用於Bourns®產品故障可能導致人身傷害或死亡的任何其他應用。請參閱法律免責聲明:www.bourns.com/docs/legal/disclaimer.pdf

媒體代理窗口:
Annette Keller
Keller Communication
(949) 947-7232
annettekeller1984@gmail.com
Bourns亞太媒體聯絡人
陳僑芬 Josephine Chen
Bourns Asia Pacific, Inc
886-2-2562-4117#138
Josephine.chen@bourns.com