Search
Languages

Bourns to Exhibit Magnetic Components and Circuit Protection Solutions for Battery Management and On-Board Charger Applications at Automotive Engineering Exposition Yokohama 2026

RIVERSIDE, Calif., May 20, 2026 - Bourns will present its portfolio of magnetic components, circuit protection solutions, and custom magnetics for automotive applications at the Automotive Engineering Exposition Yokohama 2026, Booth #521, May 27–29, at Pacifico Yokohama. Show hours are 10:00–17:00 JST daily.

The exhibit will focus on two primary application areas: battery management systems (BMS) and on-board chargers (OBC). For BMS design teams, Bourns will feature magnetic components that address DC-DC power conversion, current sensing, and EMC requirements in battery management architectures. For OBC designers, Bourns will present filtering and circuit protection components suited to the electrical requirements of automotive charging systems.

Bourns’ custom magnetics capability will also be represented, with application-specific inductors and transformers developed to meet OEM performance and package requirements.

Key Highlights at Booth #521
  • Magnetic Components for BMS — Inductors and transformers for DC-DC conversion and current sensing in battery management system architectures
  • On-Board Charger (OBC) Solutions — Filtering and circuit protection components for automotive charging system designs
  • Custom Magnetics for Automotive Systems — Application-specific inductors and transformers developed to OEM performance and package requirements
  • Circuit Protection Solutions — Components for EV powertrain and charging system protection applications
Event Details
Event: Automotive Engineering Exposition Yokohama 2026
Location: Pacifico Yokohama, Yokohama, Japan
Dates: May 27–29, 2026
Hours: 10:00–17:00 JST (daily)
Booth: #521
Pre-Registration: Automotive Engineering Exposition 2026
Bourns Exhibit Information: Bourns Tradeshows


Design engineers attending the exposition are encouraged to pre-register and visit Booth #521 to discuss application requirements with Bourns representatives.

About Bourns

Bourns is a privately held manufacturer of power electronics, resistive components, circuit protection, and sensing solutions. Founded in 1947 and headquartered in Riverside, California, Bourns serves the automotive, industrial, consumer, communications, healthcare†, and audio markets through a global network of design, manufacturing, and sales operations. For more information, visit bourns.com.

Bourns® and the Bourns logo are registered trademarks of Bourns, Inc. and may be used only with the permission of Bourns and proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners.

Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

Agency Contact:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Company Contact:
John McCarthy
Bourns, Inc.
john.mccarthy@bourns.com