Search
Languages

Bourns New TBU® High-speed Protector Family Offers Complete, Simple to Use RS-485 Interface Protection

RIVERSIDE, Calif., Novmeber 13, 2018 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced its new Model TBU-DF and TBU-DB-Q high-speed protector (HSP) device families. These extremely fast (react in <1 millisecond), very precise semiconductor-based protectors provide a simple-to-use data line protection solution that offers inherent coordination with peripheral circuitry and fewer variables that the designer has to consider.

The TBU-DF model is designed to meet the protection needs of RS-485 interfaces that are used for data collection and remote sensing in new IoT, factor and home automation applications and in process control and test and measurement equipment. The AEC-Q101-compliant Model TBU-DB-Q Series matches the protection needs of battery sensing/balancing applications such as those in new battery management systems (BMS).

"Demand for Bourns® TBU® HSPs has grown steadily over the past several years. One of the main reasons is that TBU® devices supply a single protection solution that is simple and straight-forward. Instead of possibly having to select more than one overtemperature and overcurrent solution, a TBU® HSP is able to handle multiple threats – from induced lightning surges and ESD to installation errors and cabling fault issues," said Ben Huang, product line manager for semiconductors at Bourns.

Bourns' new TBU-DF and TBU-DB-Q Series products are low capacitance dual bidirectional high-speed Electronic Current Limiter (ECL) devices offered in surface mount DFN packaging. They are constructed using MOSFET semiconductor technology. When placed in the system circuit, they monitor the current using an integrated detection circuitry that triggers during large voltage or current transient events providing an effective barrier that protects sensitive electronics.

Bourns® TBU-DF and TBU-DB-Q device families are available now, are RoHS compliant* and are IEC 61000, IEC 61000-4-2, IEC 61000-4-4 and IEC 61000-4-5 compliant. As a helpful design resource, Bourns offers an evaluation board allowing developers to easily work with and test the new TBU® HSP products. More detailed product information can be found at: www.bourns.com/products/circuit-protection/tbu-high-speed-protectors-hsps.

Bourns® and the Bourns logo are registered trademarks of Bourns, Inc. and may be used only with the permission of Bourns and proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners.

* RoHS Directive 2015/863, Mar 31, 2015 and Annex.

Bourns について

Bourns, Inc. は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf