Search
Languages

Bourns Kicks Off Significant Expansion of its SinglFuse™ Product Line with Five New Thin Film Series

RIVERSIDE, Calif., April 17, 2018 - Bourns, Inc., a leading manufacturer and supplier of electronic components, has announced the introduction of the first of many new SinglFuse™ product series the company has planned in its strategic roadmap for 2018. The significant expansion of its SinglFuse line will include advanced wire-core, ceramic multilayer and ceramic tube fuse technologies in addition to the company’s successful thin film chip fuse products. As a leading innovator of one of the industry’s most comprehensive offerings of circuit protection solutions, the planned increase in Bourns’ SinglFuse™ product families answers the growing need for robust and reliable overcurrent protection that meets designers’ higher-rated voltage (up to 600V AC) and higher-rated current (up to 100A) application requirements. Bourns will also roll out several new series of automotive-grade fuses later in the year.

 

The first of the new SinglFuse™ devices to be introduced are five new fast-acting precision and time-lag thin film fuse product series. Fast acting precision fuses are rated to open within 5 seconds at 200 percent rated current. Time lag thin film fuses open within 1 to 120 seconds at 200 percent rated current. These latest fuse products from Bourns address the increasing need for effective circuit protection in applications including PC and LCD monitors, portable memory, cell phones, digital cameras and set-top boxes.

The first five new SinglFuse™ product series include Models SF-1206FP, SF-1206SP, SF-0603FP, SF-0603SP and SF-0402FP. These single blow fuses for overcurrent protection feature current ranges from 500 mA to 7.0 A. Offered in surface mount packaging for automated assembly, these new products also help meet limited design space constraints with small, industry-standard 0402 (1005 metric), 0603 (1608 metric) and 1206 (3216 metric) footprints.

All five of the new SinglFuse™ product series are RoHS compliant*, halogen free** and available now. For more information, please visit the product page: www.bourns.com/products/circuit-protection/singlfuse-smd-fuses or contact your local Bourns Representative or Authorized Distributor.

* RoHS Directive 2015/863, Mar 31, 2015 and Annex.

** Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

Bourns について

Bourns, Inc. は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf