Search
Languages

Bourns New Model PSL Motorized Slide Potentiometers Contribute to Lower Profile Audio, Broadcast, and Lighting Console Designs

RIVERSIDE, Calif., January 5, 2018 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced the company's new low profile motorized slide potentiometer line specifically designed to meet small space constraints, longer product life and repeated automated console adjustment requirements. Offered in 100 mm and 60 mm versions, the innovatively designed Bourns® Model PSL measures just 25 mm high, enabling audio, broadcast and lighting console engineers to reduce the surface height resulting in a slim and sleek console design.

Bourns will showcase its latest slide potentiometers and the advanced capabilities of its complete line of professional audio and lighting products at the upcoming 2018 NAMM Show, January 25-28 at the Anaheim Convention Center in Bourns booth # 12506.

With the Model PSL, Bourns is answering the current trend for lower profile solutions that also meet increased power efficiency demands while maintaining high performance characteristics. Bourns designed its latest motorized slide potentiometer with a power-saving 5 VDC Mabuchi motor so it can be used with more energy-efficient circuits. The new product line also utilizes a highly durable contacting carbon resistive ink element that delivers extended wear characteristics of up to 500,000 cycles. The element design also produces very low noise output for an optimal signal-to-noise ratio that allows improved audio quality.

Available in a variety of resistance values and standard taper options, the Bourns® Model PSL motorized slide potentiometers feature a touch sense lever, a servo track option for console automation and an easy-to-use snap-in connector.

As a pricing reference, the 100 mm version of the Model PSL is $24 in quantities of 1,000 pieces, and the 60 mm version is $23 in quantities of 1,000 pieces. Both versions are RoHS compliant* and available now through Bourns qualified distributors. For additional product information, please see the data sheet and material declaration at www.bourns.com.

*RoHS Directive 2002/95/EC Jan. 27, 2003 including annex and RoHS Recast 2011/65/EU June 8, 2011.

Bourns について

Bourns, Inc. は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf