Search
Languages

Bourns Releases New Sulfur-Resistant, AEC-Q200 Compliant Thick Film Chip Resistors

RIVERSIDE, Calif., November 20, 2017 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today released two new series of thick film chip resistors that offer enhanced power ratings up to 2 W at 70 °C. The Bourns® Models CRMxxxxA and CRSxxxxA are sulfur-resistant and AEC-Q200 compliant making them well-suited for automotive driver assistant, information, entertainment and lighting applications, as well as commercial, automation, industrial, power supply and stepper-motor drive designs.

Designed to operate in harsh environments where there are elevated levels of sulfur contamination, Bourns' latest resistor series have been tested in accordance with ASTM B809-9 methods. Made using a thick film element printed onto a ceramic substrate, the resistors offer additional product lifespan benefits compared to standard film resistors when exposed to a sulfurous gas environment.

Offering broad suitability for a diverse range of applications, the new chip resistors are available in six different footprints from small 0603 (1608 Metric) up to 2512 (6431 Metric). The Model CRMxxxxA provides a wide resistance range up to 1 megohms and low resistance values from 0.05 ohms. This models' high power rating makes it an ideal solution for current sensing. In addition, the Model CRSxxxxA delivers superior pulse load capabilities for enhanced protection of today's smaller, more sensitive electronic designs.

Available now, the Bourns® Model CRMxxxA and CRSxxxxA series are RoHS compliant* and halogen free**. As a pricing reference, Model CRM0603AF (1-10 million ohms) is priced at $0.003/pc in 5,000-piece quantities. Model CRM2512AF (1-10 million ohms) is priced at $0.073/pc in 5,000-piece quantities. Model CRS0603A-F is priced at $0.016/pc in 5,000-piece quantities. Model CRS2512A-F is priced at $0.147/pc in 4,000-piece quantities. For more detailed product information, please see: www.bourns.com/products/fixed-resistors/sulfur-resistant

*RoHS Directive 2002/95/EC Jan. 27, 2003 including annex and RoHS Recast 2011/65/EU June 8, 2011.

** Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

Bourns について

Bourns, Inc. は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf