Search
Languages

Bourns Introduces AEC-Q200 Qualified Power Inductor Products Offering Exceptionally Low Resistance, High Saturation Current

RIVERSIDE, Calif., October 5, 2016 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today introduced three new series of AEC-Q200 qualified high current shielded power inductor products. The Bourns® Models PQ2614BLA, PQ2614BHA andPQ2617BHA are designed with a flat wire winding offering exceptionally low DC and AC resistance and high saturation current of over 100 A. The flat wirewound design also provides a compact, highly efficient inductance solution. These features make the new inductor products particularly well-suited for automotive power conversion applications as well as DC/DC converters, switch-mode power supplies and filtering applications in consumer, industrial, medical and communications electronics.

Boosting the overall efficiency of DC/DC converters, these inductors feature low power dissipation combined with the low core loss nature of their ferrite core construction. In addition, these devices are mounted on a plastic base designed with an extra solder pad for increased mechanical stability. The series are offered with extended operating temperature ranges from -40 to +155 °C and inductance values of 1 - 33 µH.

The Bourns® Model PQ2614BLA, PQ2614BHA andPQ2617BHA series are available now and are RoHS compliant* and halogen free**. As a pricing reference, the Bourns® Model PQ2614BLA is priced at $1.80 each in 5k piece quantities. For more information, please visit: www.bourns.com/products/magnetic-products/power-inductors-aec-q200-qualified

*RoHS Directive 2002/95/EC Jan. 27, 2003 including annex and RoHS Recast 2011/65/EU June 8, 2011.

** Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

Bourns について

Bourns, Inc. は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf