Search
Languages

Bourns Announces Higher Power Efficiency Bridge Rectifier Products for Power and Switch Mode Power Supply Applications

RIVERSIDE, Calif., August 22, 2017 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced a new series of bridge rectifier diode products designed for converting alternating current (AC) to direct current (DC) in power applications. Designated Bourns® Model CDTO269-BR1xL, this new series of surface mount bridge rectifier diodes features low power loss and high efficiency, low forward voltage, high surge capability and high reverse robustness. Because offering greater power efficiency has become a key requirement in many next-generation designs, these features make Bourns’ new bridge rectifier diodes ideal conversion devices in many switch mode power supply (SMPS), bridge full wave rectification, lighting ballasts and battery charger applications.

Bridge rectifier diodes have become popular high reliability, small size and cost-efficient solutions delivering multiple advantages. These devices offer added rectification efficiency and a higher Transformer Utilization Factor (TUF) than standard Bourns® rectifier diodes, thus requiring only a simple filtering circuit and transformer, enabling a smaller power transformer to be used.

Pricing and Availability
The CDTO269-BR1xL series from Bourns is available now and is RoHS compliant*. As a pricing reference, Model CDTO269-BR1xL is priced at $0.175 each in 15,000-piece quantities. For more detailed product information, please visit: www.bourns.com/products/diodes/rectifier-diodes

Bourns について

Bourns, Inc. は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf