Search
Languages

Bourns Expands Successful Line of Multifuse® Ultra-Low Resistance Surface Mount PPTC Resettable Fuses


Bourns® new Multifuse® MF-PSML,
MF-NSML, MF-USML series
(Click for JPG)

RIVERSIDE, Calif., July 18, 2017 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced it has expanded its successful line of ultra-low resistance Multifuse® Polymer Positive Temperature Coefficient (PPTC) resettable fuses. Bourns is introducing the new model series MF-PSML (0805 size) while adding new low-profile devices to the company's existing MF-NSML (1206 size) and MF-USML (1210 size) series products. Bourns is extensively increasing its Multifuse® product line to provide design engineers with a breadth of low-resistance overcurrent and thermal circuit protection solutions that meet their space-constrained application requirements.

Featuring small package sizes from 1210 to 0805, the expanded Multifuse® line delivers increased resettable fuse performance from higher hold currents (Ihold) up to 7.0 Amps, higher voltages (Vmax) and post trip resistance values as low as 12 mOhms for enhanced resistance stability. For example, providing ultra-low resistance values helps boost the line's current-carrying capability where one model can now achieve a 7 Amps Ihold in a compact 1210 package (MF-USML700-2). These features enable longer battery life and faster charging in today's smaller lithium-ion battery-based devices making the new models ideal resettable protection solutions for a wide range of portable electronic applications.

All the new Multifuse® models are based on Bourns' freeXpansion™ technology, which is a space-saving manufacturing process that enables smaller surface mount package sizes, while also making it possible for Multifuse® devices to handle larger currents and voltages with improved resistance stability.

"The ultra-low resistance, small footprint, and low profile all make our latest Multifuse® product series ideal protection solutions for a new generation of space-constrained portable devices including smartphones, tablets, wireless headphones, PC motherboards, USB drives and gaming consoles," said Lee Bourns, Multifuse Product Line Manager at Bourns, Inc. "And because these devices are based on Bourns' freeXpansion™ technology, they offer superior current, voltage and resistance performance over traditional PTC solutions for designs that require more advanced overcurrent and overtemperature protection."

Manufactured in a Bourns TS16949-approved facility, the latest Multifuse® PPTC resettable fuses are available now, are RoHS compliant* and UL recognized for safety requirements.

*RoHS Directive 2002/95/EC Jan. 27, 2003 including annex and RoHS Recast 2011/65/EU June 8, 2011.

Bourns について

Bourns, Inc. は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf