Search
Languages

Bourns New High Current Power TVS Diodes Deliver Performance Enhancements for High Power DC Bus Clamping Applications

RIVERSIDE, Calif., June 7, 2017 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today released a new series of high current Power TVS (PTVS) diodes that provide excellent overvoltage protection. Bourns' latest Model PTVS-M series is designed to meet the strict surge requirements in high power DC applications, especially in exposed and harsh environments. Featuring lower clamping voltage under surge, performance stability and increased reliability compared to competing technologies such as MOVs (Metal Oxide Varistors), Bourns engineered its Model PTVS-M series using silicon-based technology to deliver superior surge performance characteristics.

Offered in an SMD package, Model PTVS-M can help simplify assembly and reduce costs by eliminating the extra manufacturing step in designs where the PTVS diode is the only through-hole component on the printed circuit board. Furthermore, the innovatively-designed "overmolded" surface mount package makes it an optimal choice for automatic pick and place assembly and reflow processes. These bidirectional TVS devices are available with standoff voltages of 66 V and 76 V, with peak pulse current ratings from 3 kA to 10 kA.

Today's high power DC applications such as AC/DC power supplies used in wireless base stations and remote telemetry stations are required to meet rigorous surge standards such as IEC 61000-4-5. The new PTVS-M series from Bourns supplies robust protection, assisting designers to meet these standards by limiting overvoltage transients to specified low clamping voltages during surges.

The Bourns® Model PTVS-M series is RoHS compliant* and available now. As a pricing reference, the Bourns® Model PTVSx-xxxx-M is priced at $24.75 each in 400 piece quantities. For more information, please visit: www.bourns.com/products/diodes/power-tvs-diodes

Bourns について

Bourns, Inc. は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf