Search
Languages

Bourns Announces Three New Pro Audio Amplifier Potentiometer Design Kits

Riverside, Calif., January 12, 2011 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced three new potentiometer design kits to facilitate the development of new and upgraded professional guitar amplifiers. Based on Bourns® Models 96, 53 and PDA241, the kits provide a variety of resistance values and tapers and can also be used as a service kit for guitar amplifier service technicians. The new design kits will be showcased along with Bourns’ complete line of guitar potentiometers and other pro audio products in Bourns Booth #2992 in Hall D at the NAMM Show, January 13 – 16, 2011 at the Anaheim Convention Center in Anaheim, California.

“Bourns continues to expand its professional audio product line with innovative products and design resources that make it easier for our customers to develop the highest quality guitar amplifiers and associated pro audio equipment,” said Chuck Manzano, product manager at Bourns, Inc. “These new design kits were developed with very high performance standards to meet the pro audio requirements, and are a good resource for integrating Bourns® potentiometers to enhance the reliability and longevity of pro audio guitar amplifiers.”

The three new Bourns amplifier design kits include the following:
  • H-1203 - Model 96 Premium Amplifier Potentiometer Design Kit - contains Bourns® 5/8-inch square potentiometers with conductive polymer long-life, low noise element. The kit is populated with both linear and audio taper potentiometers of common resistance values used in amplifiers.
  • H-1205 - Model 53 Premium Amplifier Mini-Potentiometer Design Kit - contains Bourns® ½-inch square potentiometers with conductive polymer long-life, low noise element. The kit is populated with both linear and audio taper potentiometers of common resistance values used in amplifiers.
  • H-1204 - Model PDA241 Standard Amplifier Potentiometer Design Kit - contains Bourns® 24 mm potentiometers with long-life, low noise carbon element. The kit is populated with both linear and audio taper potentiometers of common resistance values used in amplifiers.
As a kit pricing reference, the Model 96 design kit is priced at $55.60 in 1-1,000 piece quantities. The Model 53 design kit is priced at $38.89 in 1-1,000 piece quantities and the Model PDA241 is priced at $13.71 in 1-1,000 piece quantities. Samples and production quantities of all three design kits are available now.

Bourns について

Bourns, Inc. は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf