Leave a message
MENU
Search
Languages

Bourns Releases Riedon™ Modular Fuse Blocks that Meet Class-T and ANL Requirements

Devices address application protection needs ranging from renewable energy infrastructure to portable power systems

RIVERSIDE, Calif., August 27, 2024 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today announced the release of its Riedon™ Class-T and ANL modular fuse blocks. The new devices are designed to address the protection needs in a broad range of applications that include industrial power systems, battery chargers, solar inverters, and battery storage systems.

A total of four fuse block product types are now available from Bourns. The product types consist of the Model FB and CFB Series, which are Class-T fuse blocks that come provisioned with a Class-T fuse selectable up to 400 A, and offer two termination options including bare wire and ring/spade connections. The other two types are the ANL fuse block Model NFB Series and the NFB2 Series that are offered in two mounting base lengths with ring/spade connectivity and can be ordered with ANL fuses from 50 A to 500 A.

These are the first Riedon™ fuse blocks to be released by Bourns. Offering flexibility and modularity to adapt to a wide range of applications, the Model FB and CFB Class-T Series fuse blocks are constructed of high-quality materials, including tinned brass terminals, fiberglass reinforced polycarbonate mounting bases, clear polycarbonate safety covers and stainless steel mounting hardware. Specifically, the compact 3.4-inch Model NFB Series fuse block features a base constructed of heavy duty phenolic where the Model NFB2 Series is 6.5 inches in length with a fiberglass-filled polycarbonate base. Furthermore, both the Model NFB and NFB2 Series ANL fuse blocks have a clear polycarbonate safety cover and stainless-steel connection and mounting hardware that provides additional product durability and operational life.

The four series of Riedon™ fuse blocks by Bourns are available now and are RoHS compliant*. For additional information, please see: www.bourns.com/products/circuit-protection/fuse-blocks.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

In April 2023, BE Services Company, Inc., a subsidiary of Bourns, Inc., purchased certain assets of Riedon, Inc., including its logo and trademarks and the right to continue to manufacture former Riedon™ products. “Riedon Logo” is a registered trademark of BE Services Company, Inc. in the United States. “Riedon” is a trademark of BE Services Company, Inc.

Über Bourns

Bourns, Inc. ist ein führender Hersteller und Zulieferer von Positions- und Geschwindigkeits-Sensorik, Schutzabschaltungslösungen, magnetischen Komponenten, Mikroelektronikmodulen, Schalttafelsteuerungen und Widerstandsprodukten. Mit Hauptverwaltung in Riverside, Kalifornien beliefert Bourns eine Reihe von Märkten, einschließlich Automobilbranche, Industrie, Haushalt, Kommunikation, nicht-lebenserhaltende medizinische Unterstützungstechnik, Audio sowie viele andere Marktsegmente. Weitere Firmen- und Produktinformationen sind erhältlich auf www.bourns.com.

Bourns® und das Bourns-Emblem sind eingetragene Warenzeichen von Bourns, Inc. und dürfen nur mit Genehmigung von Bourns und nur mit ordnungsgemäßer Anerkennung öffentlich verwendet werden. Andere aufgeführte Namen und Marken sind Warenzeichen oder eingetragene Warenzeichen der jeweiligen Eigentümer.