Search
Languages

Bourns Further Expands Sensor Line with Highly Sensitive, Accurate Pressure Sensor Designed for Extended Temperature Applications

RIVERSIDE, Calif., May 13, 2019 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today further expanded its line of environmental sensors to include a new pressure sensor. Bourns® Model BPS140 pressure sensors are based on state-of-the-art Micro-Electro-Mechanical Systems (MEMS) technology, which provides extremely accurate condition readings in a miniature package size. Designed to deliver high sensitivity/accuracy and long-term reliability, the new BPS140 pressure sensors offer extended temperature capability and certain harsh media compatibility.

Model BPS140 is a robust device with a structure that is capable of handling high pressure ranges (15 to 500 PSI) even at high temperatures. Another advantage of Bourns' newest pressure sensor design is that its structure is combined with backside pressure measurement that minimizes the number of media-sensitive wetted materials. The purpose of this backside sensing design is to ensure the measured media only touches the backside of the measurement element.

"The structure of the BPS140 provides a distinct sensor accuracy benefit because all electronic components and other sensitive surfaces are isolated from the media," said Alain Leon, Sensors & Controls Product Line Manager at Bourns, Inc. "And, by reducing the number of wetted materials, we are effectively decreasing the media sensitivity of the sensor."

Bourns' new sensor family offers stable performance over the product's lifespan, and the ability to work with a wide range of pressures offering a Total Error Band of 2.5 % FS over a temperature range of –40 °C to 150 °C (Six-Sigma process), and a lifetime drift of 0.5 % FS. These features make the BPS140 pressure sensor an ideal solution for a range of industrial, energy, heavy equipment, building & home control and medium/low-risk medical* designs.

Bourns Model BPS140 pressure sensors are available now, and are RoHS* compliant. Bourns also offers port configuration and calibration customization. For more detailed product information: www.bourns.com/products/sensors/environmental-sensors.

*Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

**RoHS Directive 2015/863, Mar 31, 2015 and Annex.

Über Bourns

Bourns, Inc. ist ein führender Hersteller und Zulieferer von Positions- und Geschwindigkeits-Sensorik, Schutzabschaltungslösungen, magnetischen Komponenten, Mikroelektronikmodulen, Schalttafelsteuerungen und Widerstandsprodukten. Mit Hauptverwaltung in Riverside, Kalifornien beliefert Bourns eine Reihe von Märkten, einschließlich Automobilbranche, Industrie, Haushalt, Kommunikation, nicht-lebenserhaltende medizinische Unterstützungstechnik, Audio sowie viele andere Marktsegmente. Weitere Firmen- und Produktinformationen sind erhältlich auf www.bourns.com.

Bourns® und das Bourns-Emblem sind eingetragene Warenzeichen von Bourns, Inc. und dürfen nur mit Genehmigung von Bourns und nur mit ordnungsgemäßer Anerkennung öffentlich verwendet werden. Andere aufgeführte Namen und Marken sind Warenzeichen oder eingetragene Warenzeichen der jeweiligen Eigentümer.