Search
Languages
Home / News / Press Releases / Press Release

Bourns Expands Motorized Slide Potentiometer Line for Professional Audio and Lighting Applications


Bourns® Model PSP60 60mm
Motorized Slide Potentiometer
(Click for JPG)

RIVERSIDE, Calif., July 12, 2017 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced it has expanded its industry-leading line of professional audio and lighting products with a 60mm motorized slide potentiometer. The feature-rich Bourns® Model PSP60 is designed to meet space constraints, longer lifespan and frequent adjustment requirements of automated professional audio mixing consoles, broadcast mixing consoles, and professional lighting consoles and controllers.

Available in a variety of resistance values (from 10kΩ to 100kΩ) and standard taper options, the Bourns® Model PSP60 60mm motorized slide potentiometer delivers superior operational characteristics. It features a long-life carbon element offering up to 1,000,000 cycles, a touch sense lever allowing for adjustments on the fly during live shows, a servo track for console automation and a snap-in connector for ease of assembly in production.

Samples and production quantities of the Model PSP60 are now available. This series is RoHS compliant*. For additional information, please see the data sheet and material declaration at www.bourns.com.

*RoHS Directive 2002/95/EC Jan. 27, 2003 including annex and RoHS Recast 2011/65/EU June 8, 2011.

About Bourns

Bourns, Inc., is a leading manufacturer and supplier of position and speed sensors, circuit protection solutions, magnetic components, microelectronic modules, panel controls and resistive products. Headquartered in Riverside, California, USA, Bourns serves a broad range of markets, including automotive, industrial, consumer, communications, non-critical life support medical (low/medium risk), audio and various other market segments. Additional company and product information is available at www.bourns.com.

Bourns® and the Bourns logo are registered trademarks of Bourns, Inc. and may be used only with the permission of Bourns and proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners.

Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

Agency Contact:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Company Contact:
David Scofield
Bourns, Inc.
(951) 781-5054
david.scofield@bourns.com