Search
Languages

Bourns Introduces High Current PTVS Diode Capable of Handling 20 kA Surge Current with Low Clamping Voltage

Higher surge handling capability helps reduce total BOM count and saves board space in high power DC line protection applications

RIVERSIDE, Calif., September 21, 2022 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today introduced a bidirectional power transient voltage suppressor (PTVS) diode designed for high power DC line protection applications. The new Model PTVS20-015C-TH is capable of handling 20 kA current surge at a low voltage of 15 V making it an ideal and effective electrostatic discharge (ESD) protection solution for applications that require high power DC bus protection.

The Bourns® Model PTVS20-015C-TH PTVS diode meets IEC 61000-4-2 Level 4 ESD protection requirements. It also features low clamping voltage at peak pulse current and assists in meeting IEC 61000-4-5 8/20 μs current surge requirements for lightning protection.

In order to support large currents such as 60 kA in next-generation applications, designers typically have had to connect many devices with low current handling capability in parallel. With a single device capable of handling 20 kA, a fewer number of devices can now be connected in parallel to achieve the same desired protection level. This reduces the total BOM count and can help save valuable space on the PCB.

Bourns® Model PTVS20-015C-TH is available now and is RoHS compliant* and halogen free**. For more detailed product information, please see: www.bourns.com/products/diodes/power-tvs-diodes

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

ボーンズ社について

ボーンズ社(Bourns, Inc.) は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf