Search
Languages

Bourns Further Expands its POWrFuse™ High-Power Fuse Product Family with New Telecommunications Model Series

New POWrFuse™ Model PF-N series meets the UL 248-1 standard and is designed for  current limiting and short circuit protection in telecom DC power distribution circuits

RIVERSIDE, Calif., July 14, 2022 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced it has further expanded its POWrFuse™ High-Power Fuse product family with a new telecommunications model series. Bourns specifically designed the POWrFuse™ Model PF-N Series to meet the requirements of the UL 284-1 standard. Supporting operation up to 170 VDC and with two PCB mounting configurations, the PF-N Series delivers superior current limiting and short circuit protection for DC power distribution circuits in telecommunication systems.

These UL recognized high-power fuses feature a 100 kA interrupting rating, up to an 80 A current rating and an operating temperature range of -55 to +125 °C.  The features of the Bourns® POWrFuse™ PF- N Series make them optimal protection solutions that help avoid costly service calls and aid in ensuring maximum system uptime.

The Bourns® POWrFuse™ Model PF- N Series is available now and is RoHS compliant* and halogen free**. For more detailed product series information, please see: www.bourns.com/products/fuses/powrfuse-high-power-fuses

“POWrFuse” is a trademark of Bourns, Inc.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be “halogen free” if (a) the Bromine (Br) content is 900 ppm or less;

(b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

ボーンズ社について

ボーンズ社(Bourns, Inc.) は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf