Search
Languages

Bourns Introduces Shielded Gigabit Ethernet/PoE+ Chip LAN Transformers for High-Speed Telecom and EMI Suppression

Two new low profile model series provide PCB layout flexibility and support Ethernet speeds up to 10 Gbps with PoE+ capabilities

RIVERSIDE, Calif., December 20, 2021 - Bourns, Inc., a leading manufacturer and supplier of electronic components, , today introduced two new shielded Gigabit Ethernet (GbE) Chip-LAN Transformer series. Bourns® Model SM453230-121N7YP and Model SM453230-231N7YP series are small, low profile and discrete solutions giving designers additional board layout flexibility compared to traditional Chip-LAN modules. In addition, Bourns' new transformers support high network speeds up to 10 Gbps, are capable of 700 mA for PoE+ and offer a temperature range of –40 to +85 °C. They are capable of 1500 VAC/60 s Hi-Pot isolation and withstanding pulse voltages of up to 2400 V, 1.2/50 μs. These advanced features make them ideal for use in high-speed telecommunication and networking devices.

The two transformers differ in inductance, insertion loss and capacitance features due to the different bit rate ranges they address. Bourns® Model SM453230-231N7YP supports 1, 2.5 and 5 GbE, whereas Model SM453230-121N7YP is 10 GbE capable. The former can be paired with Bourns® Model SRF2012A-801Y common mode chip inductor, and the latter with Model SRF2012-900YA. These small, center-tapped transformers are wound on a drum core and capped with a ferrite plate to emulate the close magnetic path of a toroid core. A center tap allows for common mode suppression even without an extra common mode filter, and the new series help reduce EMI troubleshooting efforts.

Bourns utilizes its fully automated production process for both new model series, which enhances component uniformity, quality and reliability. Also, high-volume production can be accommodated with shorter production lead times and reduced cost with this process.

Bourns® Model SM453230-121N7YP and SM453230-231N7YP GbE Chip-LAN transformers are available now and are RoHS compliant* and halogen free**. For more detailed product information, please see: www.bourns.com/products/magnetic-products/transformers-signal

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

ボーンズ社について

ボーンズ社(Bourns, Inc.) は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf