Search
Languages

Bourns Extends Rotary Encoder Line with New Model Featuring High Detent Force with Smooth Tactile Feedback

Model PEC11H is Designed for Applications that Require a Rugged Menu-Select Encoder

RIVERSIDE, Calif., June 25, 2020 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced the introduction of Model PEC11H as an extension to the company's rotary encoder product line. Bourns engineered its Model PEC11H encoder with an innovative ball/spring design that provides a strong, positive detent feel. This high force detent feature satisfies increasing end-user demands for more noticeable and smooth tactile feedback in a broad range of applications that require a rugged menu-select encoder such as in Professional Audio and Lighting, low/medium risk medical**, test/measurement and lab equipment, industrial automation controls and consumer white goods.

Bourns' new rotary encoder also features quadrature output with a 100,000 rotational cycle rating and a –25 °C to +70 °C operating temperature range. Delivering design flexibility, the Model PEC11H is offered in various resolutions and knurled and flatted shaft lengths as well as with a momentary push switch option.

The Model PEC11H encoder is RoHS* compliant, has an IP 40 dust seal rating, and is available now. For more detailed product information, please refer to the Bourns website: www.bourns.com/products/encoders/contacting-encoders

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

ボーンズ社について

ボーンズ社(Bourns, Inc.) は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf