Search
Languages

Bourns Adds Four New Model Families to its Environmental Pressure Sensor Line

RIVERSIDE, Calif., February 26, 2020 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced the addition of four new model families to the Bourns® Precision Sensor (BPS) line. Based on state-of-the-art Micro-Electro-Mechanical Systems (MEMS) technology, the four new BPS310, BPS320, BPS330 and BPS340 series are cost-effective pressure sensor solutions that feature ultra-fast response times, high resolution, and long-term stability. These features, along with the ability to work with pressure ranges from 5 to 500 psi, make Bourns' latest BPS sensors ideal for a vast array of packaging requirements and applications including industrial systems and low/medium risk medical† devices.

The Model BPS310 series is designed to provide high sensitivity/accuracy for ultra-low pressures. For gauge and pressure measurement, the Model BPS320 series offers a robust configuration in a surface mount package. The Model BPS330 series is a through-hole pressure sensor with an aluminum port for low pressure applications with an operating range up to 125 °C. With an ability to handle certain harsh medias, the Model BPS340 series is offered in a surface mount package capable of supporting pressure ranges up to 500 psi.

Bourns® BPS310, BPS320, BPS330 and BPS340 series sensors are available now and are RoHS* compliant. For additional product information, please see: www.bourns.com/products/sensors/environmental-sensors

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

ボーンズ社について

ボーンズ社(Bourns, Inc.) は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf