Search
Languages

Bourns to Showcase and Demonstrate its line of MEMS-based Environmental Sensors at Sensor + Test 2019

RIVERSIDE, Calif., June 13, 2019 - Bourns, Inc., a leading manufacturer and supplier of electronic components, will demonstrate and display its growing line of environmental sensors at Sensor + Test 2019. Bourns® standard and customizable pressure and humidity sensor product solutions are based on Micro-Electro-Mechanical Systems (MEMS) technology enabling them to deliver extremely accurate condition readings in a miniature package size.

In addition, Bourns will highlight its customization capabilities for position and environmental sensors. Attendees will also learn about Bourns Specialty Engineering & Manufacturing Services (SEMS) that provide proven technical resources for customized and cost-effective electronic solutions that help speed time-to-market for customers.

Booth highlights:

  • Working demonstrations of Bourns® BPS pressure and humidity sensors
  • High accuracy pressure sensors
    • Models BPS130/BPS140 delivers certain harsh media compatibility; capable of handling high pressure ranges (15 to 500 PSI) even at high temperatures
    • Ultra-low 0.15 to 1.0 PSI pressure sensor Models BPS110/BPS120 offer fully calibrated/compensated output for more efficient processes
  • Custom design, packaging and manufacturing expertise helps customers meet application-specific requirements
  • One of the industry’s broadest lines of circuit protection, circuit conditioning and motion control products

Where: Sensor + Test, Nuremberg, Germany
When: June 25 – 27, 2019
Location: Bourns Booth #351, Hall 5

You are invited to meet with a Bourns technical support expert to learn more about the performance, reliability and small form factor advantages of integrating Bourns BPS pressure and humidity sensors into next-generation designs. Please contact Annette Keller, 707-947-7232, annettekeller1984@gmail.com.

ボーンズ社について

ボーンズ社(Bourns, Inc.) は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf