About Us | News | Blog | My Bourns | Partner Portals | Sales | Contact | Careers |  
Products Services Applications Design Kits Library Support RoHS Training
 
Site Search       Advanced Search  
News
What's New
Press Releases
PR Images
Bourns Blog
Bourns Twitter
Tradeshows
Boilerplate
Press Contacts
 
 
 
 
 
 
2008 Press Release
Bourns Adds Highly Reliable, Long Rotational Life Rotary Position Sensor to its Trimpot Product Line
Bourns Adds Highly Reliable, Long Rotational Life Rotary Position Sensor to its Trimpot Product Line
Download Hi Res Image (JPG 828KB)
RIVERSIDE, Calif, Sep 9, 2008 — Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced the availability of a new 12 millimeter (mm) rotary position sensor. The small and highly reliable new dust-proof rotary sensor, designated Model 3382, provides long product life with its 1 million rotational cycles and IP40 seal rating. The Bourns Model 3382 is the latest addition to the company’s Trimpot product line and is designed for a wide range of space-constrained applications requiring high quality and reliability such as navigation systems, automotive power seats and mirrors, portable electronic equipment, digital cameras, industrial equipment and controls, robotic systems and home applications including mechanical compartment systems, appliances, in-wall temperature control systems and more.

“Bourns’ new rotary position sensor offers a more economical and reliable solution for many applications compared to conventional panel controls,” said Emill Melliz, Trimpot product line manager at Bourns. “The low profile, simple and elegant design gives our customers greater design flexibility, and Bourns will  extend that design flexibility with new configurations and options that will be available in the near future.”

Bourns’ Model 3382 rotary position sensor has a shaftless, surface-mount design that features exceptional performance characteristics including a broad operating temperature range (-40ºC to +120ºC), and great independent linearity (+2%) for its compact size. This device is well suited for applications that require frequent adjustment where it is necessary to control a variable output such as frequency, speed, contrast, brightness intensity, or volume control. The design is also a good solution for applications where a mechanical angular displacement is measured by the device’s proportional ouput signal. 

Pricing and Availability
Bourns’ Model 3382 12mm dust-proof rotary position sensor is available now in production quantities. As a pricing reference, the Model 3382 is offered in the price range of $1.10 to $1.20 for 1,000 piece quantities through distribution.

About Bourns

Bourns, Inc. is a leading manufacturer and supplier of automotive sensors, circuit protection solutions, magnetic products, microelectronic modules, precision potentiometers, panel controls and encoders and resistive products. Headquartered in Riverside, CA, Bourns serves a broad range of markets, including telecommunications, computer, industrial, instrumentation, automotive, consumer, non-critical life support medical, audio and various other market segments. Bourns products are manufactured according to ISO-9000 standards under Six Sigma quality programs. Additional company and product information is available at the company’s website at www.bourns.com.

Bourns® and the Bourns logo are trademarks or registered trademarks of Bourns, Inc. and may be used publicly only with the permission of Bourns and require proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners.

Agency Contact:
Annette Keller
Keller Communication
(949) 640-4811
annettekeller@sbcglobal.net
  Company Contact:
Mikelyn Bridges
Bourns, Inc.
(951) 781-5397
mike.bridges@bourns.com