About Us | News | Blog | My Bourns | Partner Portals | Sales | Contact | Careers |  
Products Services Applications Design Kits Library Support RoHS Training
 
Site Search       Advanced Search  
News
What's New
Press Releases
PR Images
Bourns Blog
Bourns Twitter
Tradeshows
Boilerplate
Press Contacts
 
 
 
 
 
 
2011 Press Release
Bourns Introduces Non-Contacting Rotary Position Sensor
Bourns Introduces Non-Contacting Rotary Position Sensor
Download Hi Res Image (JPG 828KB)
Riverside, Calif., Oct 25, 2011 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced the availability of a new non-contacting magnetic rotary position sensor which can help increase product lifespan and reliability of applications that operate in harsh and high vibration environments. Designated Bourns® Model AMS22, the sensor utilizes magnetic hall-effect technology that enables high performance operation even in severe temperature or unclean conditions. The new sensor is the latest addition to the company's sensor product line, and is designed to meet OEM requirements for a cost-effective, long life position sensor that improves reliability. Bourns® non-contacting rotary position sensor is an ideal solution for value and actuator position feedback, camera and antenna location identification and precision positioning requirements in a wide range of applications that include medical diagnostic and general industrial equipment.

"The release of Bourns' new non-contacting rotary position sensor is in direct response to our customers' requirements for solutions that help extend product life and reliability in an increasing number of applications that must operate in extreme environmental conditions," said John Kelly, General Manager Industrial Market at Bourns, Inc. "Designed to maintain its magnetic orientation even during redundant mechanical operation, this new sensor provides an excellent solution to applications that are dormant for extended periods of time but require precise position information on demand. Bourns is committed to continued development of solutions that help our customers solve tough technology issues. We are not just delivering a new product, we are launching a new technology platform that will meet the existing and future needs of the Industrial, Consumer and Automotive markets we serve."

Bourns' non-contacting rotary position sensor helps improve product longevity up to fifty million cycles depending on the product and particular application. The new sensor has an analog single output from 0.1 to 4.9v, with an effective electrical output of 340 degrees and is programmable up to 360 degrees. The analog output features a 12 bit resolution and comes with independent linearity of 0.5% or 0.3%.

Pricing and Availability
The new non-contacting rotary position sensor is available now in production quantities. As a pricing reference, the Bourns® Model AMS22 is offered at $12.50 for 10,000 piece quantities through distribution.
About Bourns

Bourns, Inc. is a leading manufacturer and supplier of automotive sensors, circuit protection solutions, magnetic products, microelectronic modules, precision potentiometers, panel controls and encoders and resistive products. Headquartered in Riverside, CA, Bourns serves a broad range of markets, including telecommunications, computer, industrial, instrumentation, automotive, consumer, non-critical life support medical, audio and various other market segments. Bourns products are manufactured according to ISO-9000 standards under Six Sigma quality programs. Additional company and product information is available at the company’s website at www.bourns.com.

Bourns® and the Bourns logo are trademarks or registered trademarks of Bourns, Inc. and may be used publicly only with the permission of Bourns and require proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners.

Agency Contact:
Annette Keller
Keller Communication
(949) 640-4811
annettekeller@sbcglobal.net
  Company Contact:
Mikelyn Bridges
Bourns, Inc.
(951) 781-5397
mike.bridges@bourns.com